Manufacturing and construction workers looking at laptop outside on site.

Standby Power for  Manufacturing

Generac Industrial Power Provides "Backup" for Manufacturing Facilities

The backbone of America relies on power generator manufacturers.  Everything from vehicles to medical equipment to furniture to electronics to aerospace to pulp and paper mills to plastic molding, and so much more.  When the power goes out due to grid failures or weather, you could suffer inventory losses, equipment failure or miss "just-in-time" delivery dates resulting in the loss of thousands or even millins of dollars in revenue.  For many processes, loss of power spoils the end product which now becomes scrap and has to be disposed.  Staff members working overtime hours will not be able to compensate for the waste.

With all that heavy lifting, you need genuine power to keep you poerating during and outage.  No worries - Generac Industrial Power provides the muscle you need.

Rely on Generac Industrial Power

Generac offers a vast array of backup/emergency and prime power solutions to meet your needs.  We offer low kW generators ideal for smaller manufacturers such as tool and die shops and commercial printers.

Generator Product Wattage Comparison

At the same time, we can deliver multi-megawatt solutions designed to keep large operations running smoothly.

Providing Big Power: 750kW - 3.25MW Generators

The Generac line of 750kW - 3.25MW industrial diesel generators combines the precise components, designed, manufactured and supported by a single source - Generac Industrial Power.  We control every part of the production and testing process - engines, alternatoes, control systems, enclosures and base tanks.  These components are all specifically designed and built to meet the highest reliability and performance standards.

Inside every Generac generator is over half a century of innovation hard at work.  Before a design goes into production, we test ever aspect of it in our own state-of-the-art R&D facility, to UL2200 standards.

Need More Power?  Consider MPS

While many facilities can be served by a single large kW generator, your operation may be growing and need more flexibility and scalability for backup power.  Generac's disruptive Modular Power Systems (MPS) allow you to easily add generators as your power needs grow.  Our MPS features integrated on-generator paralleling so there is need for expensive and large third-party switchgear.  This means you can purhase the kWs that meet your power needs now, and grow as needed.  This allows you to invest more of your initial capital in equipment or machinery that serves your core business functions.

While many facilities can be served by a single large kW generator, your operation may be growing and need more flexibility and scalability for backup power.  Generac's disruptive Modular Power Systems (MPS) allow you to easily add generators as your power needs grow.  Our MPS features integrated on-generator paralleling so there is need for expensive and large third-party switchgear.  This means you can purhase the kWs that meet your power needs now, and grow as needed.  This allows you to invest more of your initial capital in equipment or machinery that serves your core business functions.

Manufacturing worker creating parts for a generator.

Fuel Choices to Meet Your Needs As Well as Growing Emissions Concerns

With best-in-class engines for harsh environments, Generac Industrial Power diesel generators feature proven injection technology with increased tolerance for dirty fuel, common in generator applications, ensuring dependable performance.

While diesel has been the traditional duel choice, many manufacturers are considering their carbon footprints and taking steps to become more eco-friendly.  Should your company be considering these options, Generac manufactures generators that run on natural gas, which has significantly refuced emissions compared to diesel.

We also offer pioneering bi-fuel generators, which start on diesel and transition to natural gas as load is applied. This assures you have the initial power to take the heavy starting load of motors or other equipment, while providing significantly longer runtimes and less diesel fuel storage. It's a win-win-win.

Cranes lifting Generac Industrial Power generators on location.

Enclosures Built to Survive in Harsh Environments

Inhouse Built Industrial Generators

The enclosures for our large industrial generators are all built in-house at one of our USA-based manufacturing facilities.  We understand what it takes to not only build a generator that lasts, but one that is built to handle the conditions on your site.  Manufacturing our own enclosures ensures your unit combines heavy-duty durability, noise reduction, weather resistance and single source responsibility.

Immense Support from Generac Industrial Power

Factory-trained technical sales experts help with the design, sizing and specification of an industrial generator that fits your application.  This may include the addition of specific components such as larger alternators or remote controllers to meet your needs.  Our nationwise industrial sales and service network supports you completely - installation, commissioning, diagnostics - and is available 24/7/365 for emergency response, warranty service and scheduled maintenance programs. 

At Generac, one of the largest diesel generator manufacturers, we understand the challenges manufacturers face because we are one, too.  You can be assured - we work as hard as you do.