Founded in 1959, Generac was the first to engineer affordable home standby generators, along with the first engine developed specifically for the rigors of generator use, and is now the #1 manufacturer of home backup generators. Generac manufactures the widest range of power products in the marketplace including portable, residential, commercial and industrial generators. We are also the leading designer and manufacturer of manual and fully automatic transfer switches and accessories for backup power applications up to 2 MW.
Our Generac Mobile line of powerful, high-quality light towers, trailer-mounted mobile generators and combination units are designed and built for a variety of industries and the most demanding environments.
Generac also pioneered the residential power washer category, putting the power to clean into the hands of homeowners. Today, Generac features a full line of innovative, industry-leading power washers suitable for virtually any application, including the toughest commercial and industrial environments.
At Generac, we protect the things that power your life by providing quality, affordable power solutions.
Get a glimpse inside Generac operations across all facilities.
Generac is committed to developing a long-term vision that promotes environmentally responsible products, processes, and partnerships. We offer product options that allow our customers to shrink their ecological footprint when backup energy use is required. Manufacturing processes are implemented with the goal of minimizing environmental impact by reducing the amount of materials used and emissions produced. Partnerships are sought with organizations and stakeholders to further the development of sustainable technologies. By adhering to these principles, we strive to be a positive contributor of sustainable growth in our industry.
Click here to read Generac’s latest ESG report.
Be a part of Generac Nation to receive our quarterly newsletter packed with Generac products promotions, giveaways, power outage tips, and more! Sign up now to receive instant access to past articles!