Business Benefits for Bi-Fuel™
Mitigate Risks with Redundant Fuel Options
Despite the perceived value of having diesel fuel on-site for reliability, power outages can damage infrastructure and make diesel refueling difficult or impossible. Generac BI-FUEL™ generators mitigate refueling issues by operating primarily on utility-supplied natural gas.
That means less diesel fuel is required on-site, and the diesel fuel that is available will last longer during an outage since running times are greatly extended. And, since the natural gas infrastructure tends not to be affected by the same conditions that lead to power outages, fuel reliability is improved.
The good news is that should something happen to interrupt the natural gas supply; Generac BI-FUEL™ generators can seamlessly run on 100% diesel fuel. You can end the debate between a natural gas vs. diesel generator.