Phase 1 of the project was installing solar PV to offset a portion of the facilities load during the day. Due to the interconnect agreement, the facility is not allowed to export power, so ARC actively curtails the PV production as required when PV is greater than load.
The system will be allowed to run for several months to record load data in the ARC database which will then allow Generac to properly size additional PV and energy storage to allow resilient backup power at the facility during weddings and other events.