Inside a Generac Industrial Power product.

Natural Gas Fuel  Reliable. Cleaner. Smarter.

Looking for an inspired generator solution?

Consider natural gas fuel. While working with natural gas was problematic years ago, new technologies have increased the durability and reliability of these gas gensets. Combine that with the reduced air emissions and smaller carbon footprint and you have a winning solution for many applications.

Two Generac Industrial Power generators outside of building.

Award Winning Technology

Our experience and innovative technological advances in natural gas generators have actually won us back-to-back awards from Frost and Sullivan as “The Natural Gas Generator Company of the Year”. In addition, our 500 kW natural gas generator recently earned a Silver Award from the readers of Consulting-Specifying Engineer magazine.

Silver Award Winner of 2016 engineer product of the year

More About Natural Gas

Due in large part to the increased domestic production and use of natural gas, the United States has become a recognized leader in clean energy. Abundant, affordable natural gas has supported manufacturing growth, improved air quality, and lowered carbon dioxide emissions to levels not seen in decades. (Source: Dave McCurdy President and CEO American Gas Association)

Built to Last by the Best in the Business

Generac Spark-ignited Engines Engineered Specifically for Backup Power

We have a single-minded focus to provide engines designed to do one thing—generate backup power. To ensure reliability and long life, we manufacture our own-spark ignited engines from the block-up. Applying natural gas (rather than diesel) to spark-ignited engines requires advanced engineering expertise and Generac has more than five decades of experience that goes to work for you every day.

Protection from the Elements

Generac manufactures its own generator enclosures to ensure each unit combines the highest level of durability with the latest engineering advancements in noise reduction, weather resistance, and streamlined design. In addition to our standard enclosures, we also offer high performance and extreme performance enclosures.

Employee working on a natural gas machine.
Rugged Base Frames

Generac’s heavy-duty base frames ensure accurate alignment between the engine and alternator at all times. Oil and water drain points are situated for easy access. Vibration isolators contribute to smooth operation. Power cable stub-ups are positioned for easy installation.

PowerManager® Integrated Controls

PowerManager digital controls* let you monitor and control key elements of your generator system with the touch of a button or click of a mouse. Features like constant monitoring capabilities, adjustable parameters, and built-in protective alarms help provide the highest level of reliability.

*Not available on QuietSource products.

Optimized Alternator Performance

Generac industrial alternators are machine wound, machine inserted, and machine varnished for the ultimate in consistency. Form winding and stack bracing ensures reliable performance. Rotor spin balancing eliminates vibration, and vented rotors contribute to cooler operation, longer life, and enhanced efficiency.

Construction workers outside a warehouse with a Generac generator.

Generac Provides Sales, Design, Installation and Service Support

Commercial, industrial, and mission critical facilities rely on Generac Industrial Power every day. From 10 kW convenience stores to multi-megawatt wastewater systems, Generac Industrial Power has over half a century of experience designing, installing, and commissioning industrial power projects across North America. These projects meet life safety building codes.

If you have questions about our gaseous generators or just want to learn more, contact one of our Commercial and Industrial Distributors. Our worldwide network has factory-trained and certified technicians with trusted expertise in system design, sizing, installation, commissioning, diagnostics, and repairs.