Cats and dogs
Keeping cats, dogs and other mammals comfortable during an outage can be as simple as providing plenty of blankets for snuggling or shady spots for chilling out. Treat them the same way you’d treat yourself: with plenty of food and water, battery-operated fans or small heaters and more. But pets that live in controlled environments, like aquariums or reptile habitats, are more of a challenge. Ideally, you’ll have some form of backup power: a home safe backup generator, portable generator, power bank or extra batteries will all do the trick. Depending on your power needs, you could even use a laptop or car battery in a pinch.
Fish
Fish rely on heaters, filters, lights and CO2 systems to survive—equipment that runs on electricity. When the power goes out, they’re left in the lurch. Don’t panic. Fish are adaptable, but sensitive to sudden changes. If you don’t have a backup on hand, your safest bet is to wait it out. Don’t dump flakes in the water or attempt to adjust the temperature with hot or cold water. Your fish will be ok for one to two hours without intervention, and you can use that time to find a power source. Once you have one, use it to run oxygen for an hour or so. Pay close attention to your fish—if they’re gasping for air, add oxygen earlier or more often. If you’re stuck inside and can’t find any source of power, you can get creative with last-resort manual techniques.
Reptiles
For reptiles, the challenge is to keep them warm. First, consider moving them to a smaller enclosure that’ll be easier to heat. Then, you can insulate their habitat with blankets or cardboard, using hand warmers or hot water bottles to keep their home toasty. (Take care to wrap your heat source in a towel or cloth. Direct contact with a hot surface could hurt your pets.) You can also use the fireplace, stove, candles and even your own body heat to warm them. Finally, don’t feed them. It might seem counterintuitive, but reptiles need heat to digest their meals. If conditions aren’t ideal, it’s better to wait for power to return before treating them with a snack.
Birds
Birds are finicky too. When outages strike, you might be tempted light some candles or heat your stove for warmth and light. Unfortunately, birds are very sensitive to fumes—you might’ve heard the phrase “canary in a coal mine.” That said, fire isn’t completely off-limits so long as you take proper precautions. Keep your birds in another room, far away from any emissions, and they should be ok. Stick with other heat sources to keep them warm. Unlike reptiles, birds will appreciate some extra snacks. They have high metabolisms, and they’ll need the calories to stay warm.
If heat, not cold, is the issue, do your best to keep your birds cool. Move them into the shade, offer them plenty of water and consider opening a couple windows to provide a breeze (making sure they’re not in the direct path of a draft). You can also give them a bath or bottle misting to help them chill out.
Stay vigilant after the power returns.
When the lights click back on, you can breathe a sigh of relief. But don’t rest yet—check your pets for lingering signs of stress, injury or illness. Significant changes in their behavior might be a cause for concern. Keep a close eye on them, and if it feels serious, call their vet. You know your pet best.
Don’t forget to restock your emergency kit in the days after. If you were missing something this time, make sure it’s on hand for the next outage.