Emergency Preparedness

Hurricane Preparedness Guide: Everything You Need to Know

15 Min Read May 04, 2026

2026 Hurricane Forecast:
Know what could be coming your way

A new hurricane season brings a familiar question: are you ready if the chaos crosses your path? While no two storm seasons are the same, your priority remains unchanged - to protect what matters most.

For the 2026 hurricane season, Colorado State University (CSU) Tropical Meteorology Project Team predicts below-normal activity that could yield:

13 Named Storms 13 named storms
6 Hurricanes 6 hurricanes
2 Major Hurricanes At least 2 major hurricanes (Category 3 or higher)

Data Source: CSU Tropical Meteorology Project Team

Even with a below-normal outlook, it only takes one landfall - along the Atlantic or Gulf coast - to make it an active season where you live. And recent history is a clear reminder of the devastation that hurricanes can deliver even far beyond the shoreline.

Hurricane Helene & Milton caused:
 
9.5 million
power outages at peak
$113+ billion
in damages
important note:
A quieter forecast may feel reassuring, but preparation isn’t about predictions. It’s about being ready for what’s possible well before these 2026 storms have a name.

Are you in a high-risk area?

Hurricanes don’t have to make landfall where you live to disrupt your routine - or your life. NOAA’s “hurricane return period” analysis estimates how often a hurricane can be expected to pass within 50 nautical miles of a specific location.

The highest-frequency areas for hurricanes of any category include coastal North Carolina, south Florida and southeast Louisiana, about every five to seven years.

Coastal Risk Areas in United States

Probabilities for at least one major hurricane landfall (Category 3-4-5) in 2026:

  • 32% for the entire U.S. coastline.
  • 5% for the U.S. East Coast, including the Florida Peninsula.
  • 20% for the Gulf Coast, Florida panhandle to Brownsville, Texas.
Keep your whole home standby generator ready to power on

Keep your whole home standby generator ready to power on

Before Mother Nature throws her worst your way, it’s best to ensure your generator is ready to power your home - and your comfort.

  • Clear debris and any obstructions away from the generator with at least 3 ft. of clearance on each side.
  • Ensure the inside of the enclosure is free of debris (leaves, sticks, dirt, etc.).
  • Inspect lines and connections for fuel or oil leaks.
  • Inspect the entire fuel system for signs of corrosion or other concerns.
  • Be sure to check your battery for proper charge and clean terminals, air filter, spark plugs and sediment trap.
  • Watch the oil level, especially if your generator is running continuously.

The real cost of power outages

Lodging costs
per night
$110
 
Restock
refrigerator
$250
 
Flooded
basement
$26,807

Hotels.com, FEMA.gov “Big cost of flooding”
http://www.fema.gov/media-library/assets/documents181549, USDA: https://www.usda.gov

The best time to prepare for a storm is well before it happens. Stay ahead of any weather event with the supplies and information you need to keep you and yours ready for anything.

Start now

  • Identify the safest location in your home to wait out a storm and review emergency plans for evacuation and local authority recommendations.

  • Identify your nearest evacuation centers. As an alternative, create a list of options with friends outside of the forecasted storm area.
  • Create a communication plan, designate primary and backup meeting places and gather maps in case mobile service is down.
Photograph Your Possessions

Photograph your possessions

  • Start with your most expensive items (both inside and outside the home).
  • Show items closeup and in their location with the date and value.
  • Include wills, proof of insurance, receipts and other vital documents.
Carbon Monoxide Alarm

Working smoke and carbon monoxide (CO) alarms save lives

  • Interconnected CO alarms are best; when one sounds, they all sound.
  • Install both on each level and outside separate sleeping areas.
  • Test alarms monthly and replace batteries as needed.

Never ignore an alarm. Get outside immediately when it sounds. Then call 911.

Source: www.cpsc.gov

Do you have an emergency kit?

Get prepared before the unexpected—use our printable checklist to build a complete emergency kit. Download and keep it handy so you’re ready when it matters most.

View / Download / Print

Ready for the storm. And the days that follow.

Storms are unpredictable, but they don’t need to catch you off guard. Here are a few simple ways to stay one step ahead.

Food safety

According to the U.S. Department of Agriculture, food in your refrigerator is safe to eat for only four hours without electricity. Beyond that, they recommend discarding meat, poultry, fish, eggs and leftovers.

However, a full freezer will hold a safe temperature for 48 hours (24 hours if half full). These times are only true if the appliance door remains closed. It’s important to adhere to these guidelines during and after a power outage:

  • Keep your refrigerator closed.
  • Use a thermometer to check if food is 40 degrees or below before consuming.
  • Consider backup options to power your refrigerator, especially during long outages.

Child safety

Help keep children as calm as possible before, during and after a hurricane with a little guidance and reassurance to ease fears and stress.

Constant communication
  • Talk about your safety or evacuation plans before a storm arrives. 
  • Let them help gather supplies and feel part of the process.
  • Keep in constant communication during a storm or hurricane. Talk through what you’re experiencing and share your plans for what happens after the storm.
Child-friendly evacuation kit
  • Pack water, snacks and first aid items including bandages and antibiotic ointment.
  • Include toys, games and other comfort items that don’t require power.

Living in an apartment or condo?

Consider Portable Power Stations: they produce zero emissions, are safe for indoor use and the GB2000 can power a 120W refrigerator for up to 24 hours*

View our Portable Solutions

*Model and use case can vary
Generac portable power station

Pet safety

When preparing for a hurricane, keep your four-legged family members in mind as well. The ASPCA estimates one third of cat and dog owners don’t have a pet disaster plan in place for their animals, leading to last-minute stress during evacuation situations.

please remember:
Not all hotels or shelters accept pets. If you decide to stay home, continue to monitor any evacuation notices.
Emergency kits should include:
  • 7 days food and water (with a can opener, if needed).
  • Medication for one week.
  • Pet carrier / kennel.
  • Extra leash.
  • Photo of you and your pet together to prove ownership.
  • Pet ID tags, rabies vaccination tag and collar.
  • Medical or vaccination records to share with a pet friendly shelter.
Additional tips include:
  • Getting your pet microchipped (talk to your vet).
  • Placing a rescue alert sticker on your door if you shelter in place letting responders know there’s a pet inside.
  • Writing “EVACUATED” on any alert sticker if your choose to leave.
  • Slowly reintroducing your pet(s) to a disheveled home if you evacuated to reduce stress and unknown dangers.
Generac portable power station

If you have an aquarium

To maintain the delicate balance in an aquarium, you must keep your filtration system and heater running 24/7. Whether the outage lasts for a few hour or a few days, here are several things you can do to minimize damage:

  • Unplug your filter and rinse it before restarting.
  • Maintain stable water temperature by covering the tank with a blanket.
  • Make up for lost oxygen with a battery-powered air pump.
  • Have a Generac generator to keep the power on.

Before the storm

Make the most of your preparation time
  • Turn your refrigerator and freezer to the coldest setting.
  • Fill bathtubs and large containers with water for sanitation purposes.
  • Turn off and properly secure outdoor grill propane tanks.
  • Unplug small appliances in the rooms you do not plan to use during a storm.
  • Charge cell phones.
  • Check the yard and landscaping for any trees that should be trimmed, clear gutters and bring in outside items if they can be picked up by high winds.
  • Fill gas cans in the event of an evacuation or to run a portable generator.
  • Use hurricane shutters or board up windows and doors with 5/8 inch plywood.
  • Reinforce garage doors using a door bracing kit.
How to Prepare Before the Storm

How long do you have to prepare?

Hurricane Watch
When a watch is issued
This means conditions are favorable to produce potentially dangerous weather in your area within 48 hours or less.

Hurricane Warning
When a warning is issued
Severe conditions have been observed and potentially dangerous weather is imminent in or near your area within 36 hours or less.

During the storm

Should you stay or should you go?
During the Storm: Consider Leaving or Evacuating
Consider leaving
  • Prepare to depart if you live in a manufactured or mobile home, or your home was built prior to current hurricane building standards.
  • Leave if your home is vulnerable to a storm surge or flooding.
  • If an evacuation has been issued, leave immediately.
When evacuating
  • Know where you’re going. Plan primary and alternative routes ahead of time.
  • Create an evacuation destination with a backup location in mind.
  • Listen to orders at least twice to determine driving directions.
  • Grab your emergency kit in anticipation of long power outages.
  •  Bring backup maps/directions in the event mobile services aren’t available.
  • Unplug appliances, turn off water at the main valve and deactivate electricity at the breaker box.
  • Pack your vehicle and go to your designated evacuation spot or backup location.
  • Turn on the radio to stay tuned to emergency bulletins.
  • Stick to evacuation routes.

When Sheltering in Place
  • Cover all windows with permanent storm shutters or 5/8-inch exterior grade marine plywood.

  • Take refuge in a small, interior room or closet in the lowest level of your home. Avoid windows and glass doors.

  • Stay tuned to updates and have a battery-powered emergency radio on hand.

  • Save phone battery as much as possible.

  • Unplug all devices form outlets during outages to reduce power surge damage.

  • If flooding nears the home, turn off all electricity.

  • Evacuate immediately if given the order OR if the home is damaged.

Never operate a generator indoors

(including a garage) even with windows open. Carbon monoxide gas is odorless, colorless and can be deadly within minutes.

Portable generator being moved outdoors

After the storm

Return safe and with a plan to resume everyday life
  • Do not return before local authorities recommend.

  • Whether sheltered in place or returning, stay alert for potential damage and dangers -- including post-storm rain that can produce flooding.

  • If your home was seriously damaged, leave immediately and report it to local authorities.
  • If you suspect a gas leak, leave immediately and report it to local authorities.
  • Check on neighbors.

  • Report downed power lines to the utility company and local police/fire departments.

  • Take photos of your home, yard and street.

  • Contact your insurance.

  • Do not drive on closed roads - avoid flash-flooding or downed power lines.

  • Consider hiring contractors to clean up large debris to avoid personal injury.

  • Keep receipts for possible reimbursement through insurance or government programs.

  • If power is out, unplug all major appliances before turning the electricity back on to minimize possible surge damage.

  • If your home flooded, have a professional electrician check the residence before turning electricity on.

  • Save all phone calls for emergencies. Phone systems are often downed or busy after a disaster. Use text messages or social media to communicate with family and friends.

In case of extended power outages

  • Have alternate plans for refrigerating medicines or using power-dependent medical devices.
  • Keep freezers and refrigerators closed. 
  • Only use portable generators outdoors and far away from windows, doors and vents. 
  • Disconnect appliances and electronics to avoid potential surge damage. 

For whole home generator extended runtime duration and information, check your owner’s manual or contact your local dealer.

Related articles