Get up to $9,000 back*  on the installation of a new PWRcell®

 If you are a Duke Energy customer residing in North Carolina and are thinking about adding rooftop solar panels to your home, you should consider adding a PWRcell battery storage system.  Not only will this allow you to store clean, solar energy – but you may be eligible to receive up to $9,000 back from the installation cost as a one time incentive from the Duke Energy PowerPair Program.

 

What value does a Generac PWRcell system provide?

 

  • Reduce your electric bill

  • Provide backup power during utility power outages

  • Help support your local community by providing energy back to the grid (and get paid for it!)

What are the potential savings?

 

PowerPair one-time incentive up to $9,000* back for installation of new PWRcell
*assumes PWRcell model M5 (15 kWh) or higher when paired with at least 10 kW AC of solar

Power Manager & Energy Wise participants can earn an additional $420** of utility bill credits annually by enrolling.
**assumes PWRcell model M7 (7.6 kW, 21 kWh) or higher

Reduce your utility bill by storing excess solar energy throughout the day and offset your demand when electricity is expensive

Every home is different.  Sign up to learn how you can save with a PWRcell battery storage system 

 

How do I apply?

1 icon Apply

  1. Work with a Duke Energy approved PWRcell dealer to help you select the appropriate PWRcell system for your home.
  2. PWRcell dealer/installer will submit an interconnection request on your behalf and provide you with necessary details for you to submit a PowerPair application with Duke Energy.

2 icon Install

  1. Once you receive an approved interconnection and PowerPair incentive reservation from Duke Energy, you may work with your PWRcell dealer/installer to install your new system.

3 icon Connect & Receive Incentive

  1. Once your installation is complete, you will submit information about your installed system here.
  2. will validate the system information, confirm that all other eligibility requirements have been met, and mail you a check.

Both existing and new PWRcell installations are eligible to earn up to $420 per year by enrolling in the Duke Energy Power Manager / Energy Wise program.

 

Learn How I Can Save

 

Frequently Asked Questions

*These Frequently Asked Questions provide information about Duke Energy's programs, but customers should see Duke Energy program details, terms and conditions for full information.  To the extent any of this information is construed as varying from Duke Energy's terms and conditions, the Duke Energy terms and conditions control.

  • Customer must own or occupy and get owner's consent of the premise(s) where the PWRcell is installed.
  • Customer must be installing the eligible equipment for the first time – additional battery models to an existing PWRcell installation are not eligible for Duke PowerPair incentives.
  • PWRcell must be installed by Duke Energy trade ally and will be subject to inspection and verification upon request of Duke Energy.
  • Installer must be Duke Energy-approved prior to submitting an application for a PowerPair incentive for the installed equipment
  • The installed equipment must comply with interconnection standards and maintain Internetconnectivity to provide required operation and operating characteristic data.  

To find out more, fill out this form to get connected and talk to a trade ally & PWRcell dealer. See Duke Energy's full Program Details here.

  • Enrolling in Power Manager/EnergyWise Home is a simple way to help your community by letting Duke Energy more effectively manage energy on the electric grid, plus you receive monthly bill credits for participating.
  • Duke Energy’s Net Metering Bride Rider rate, which could be more favorable for your solar savings, is only available for customers enrolled in Power Manager/EnergyWise Home.

  • Click here to sign up for the program

  • Participating in Power Manager/EnergyWise Home helps decrease the use of less efficient and more expensive energy sources to support the grid.
  • Participating in the EnergyWise Home/Power Manager program allows Duke Energy Progress/Carolina to understand and sometimes use a customer’s battery to support operation of the grid.

  • Duke Energy will deploy up to 36 battery control events per year, with a minimum of 30 events
    • December – March: Up to 18 times
    • May – September: Up to 9 times -- April, October and November: Up to 9 times
  • Customers may opt out of up to four events per year
    • If customers opt out of more than four events in a year, their continued eligibility and participation in the program will be evaluated by Duke Energy and customer may be removed from program
  • Events will be called within a 48-hour period and may include a pre-charging event, hold charge steady, discharge, adjustment of user settings and return of settings to preset values. Event charge and discharge will each typically range from 1 to 3 hours. See Duke Energy's program terms and conditions here

PWRcell owners can select their desired Minimum Reserve Capacity through the PWRview application. The battery will not be discharged below this level during program events, leaving charge remaining to respond to utility power outages.

  • The Net Metering Bridge Rider associated with the Power Manager / EnergyWise Home programs may provide additional time of use savings, but discharge events scheduled by Duke Energy during non-peak hours could affect these savings  

Click here for more information

  • If you're also applying for PowerPair, select the Net Metering Bridge Rider when submitting your interconnection request with Duke Energy.
  • If you're an existing PWRcell customer, sign up here

Yes. To do so, select the Net Metering Bridge Rider when submitting your interconnection request with Duke Energy.

You may choose to only participate in PowerPair. To do so select the Residential Solar Choice Rider when submitting your interconnection request with Duke Energy.

Duke Energy PowerPair Program Incentive Breakdown  

 

Battery Make Battery Model Usable Rated Capacity (kWh) Nameplate Capacity Continuous Discharge (kW) Potential One-Time Installation Incentive**  
Generac PWRcell M3 9 kWh 3.4 kWh $7,200
Generac PWRcell M4 12 kWh 4.5 kWh $8,400

Generac

​ PWRcell M5 15 kWh 5.6 kWh $9,000

 

Duke Energy Power Manager / EnergyWise Program Incentive Breakdown  

 

Battery Make Battery Model Usable Rated Capacity (kWh) Nameplate Capacity Continuous Discharge (kW) Monthly Bill Credit Annual Potential Bill Credit
Generac PWRcell M3 9 kWh 3.4 kWh $15 $180
Generac PWRcell M4 12 kWh 4.5 kWh $20 $240

Generac

​ PWRcell M5 15 kWh 5.6 kWh $25 $300

Generac

​ PWRcell M6 18 kWh 6.7 kWh $30 $360

Generac

​ PWRcell M7 21 kWh 7.6 kWh $35 $420

Generac

​ PWRcell M8 24 kWh 7.6 kWh $35 $420

Generac

​ PWRcell M9 27 kWh 7.6 kWh $35 $420

Generac

​ PWRcell M10 30 kWh 7.6 kWh $35 $420

Generac

​ PWRcell M11 33 kWh  7.6 kWh $35 $420

Generac

​ PWRcell M12 36 kWh 7.6 kWh $35 $420